Each I/O is displayed based on a tree-structure representation. The structure is the counterpart of the formatting used in the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger to define I/Os address within the I/O editor (see Modify Input/Output).
Figure 6-6: I/Os Displayed in Object Tree
I/O value can be displayed according the following formats:
See also Custom Input/Output Editor
|
Copyright © 2015 Kollmorgen™ |
|